MW.MODEL#.ACTIVE

Description

This command indicates to the user which MechaWare models run. The value of the command indicates whether the model is active (1) or disabled (0).

Models 1-4 are Factory Models loaded by Kollmorgen. Models 5-8 are User Models.

Example

Get the Model 1 state

--> MW.MODEL1.ACTIVE
1

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read Only
Description Gets the operating state of the MechaWare model
Units N/A
Range 0-1
Default Value 1
Data Type Integer
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

MW.MODEL1.ACTIVE

30e0h

01h

Unsigned8

-

-

Read only

No

MW.MODEL2.ACTIVE

30e0h

02h

Unsigned8

-

-

Read only

No

MW.MODEL3.ACTIVE

30e0h

03h

Unsigned8

-

-

Read only

No

MW.MODEL4.ACTIVE

30e0h

04h

Unsigned8

-

-

Read only

No

MW.MODEL5.ACTIVE

30e0h

05h

Unsigned8

-

-

Read only

No

MW.MODEL6.ACTIVE

30e0h

06h

Unsigned8

-

-

Read only

No

MW.MODEL7.ACTIVE

30e0h

07h

Unsigned8

-

-

Read only

No

MW.MODEL8.ACTIVE

30e0h

08h

Unsigned8

-

-

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

MW.MODEL1.ACTIVE

2815

AFF

Unsigned8

Read Only

-

MW.MODEL2.ACTIVE

2816

B00

Unsigned8

Read Only

-

MW.MODEL3.ACTIVE

2817

B01

Unsigned8

Read Only

-

MW.MODEL4.ACTIVE

2818

B02

Unsigned8

Read Only

-

MW.MODEL5.ACTIVE

2819

B03

Unsigned8

Read Only

-

MW.MODEL6.ACTIVE

2820

B04

Unsigned8

Read Only

-

MW.MODEL7.ACTIVE

2821

B05

Unsigned8

Read Only

-

MW.MODEL8.ACTIVE

2822

B06

Unsigned8

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

MW.MODEL1.ACTIVE

2815

Unsigned8

Read Only

-

MW.MODEL2.ACTIVE

2816

Unsigned8

Read Only

-

MW.MODEL3.ACTIVE

2817

Unsigned8

Read Only

-

MW.MODEL4.ACTIVE

2818

Unsigned8

Read Only

-

MW.MODEL5.ACTIVE

2819

Unsigned8

Read Only

-

MW.MODEL6.ACTIVE

2820

Unsigned8

Read Only

-

MW.MODEL7.ACTIVE

2821

Unsigned8

Read Only

-

MW.MODEL8.ACTIVE

2822

Unsigned8

Read Only

-

Related Topics

MW.MODEL#.STATE